Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
DF59S-SN-Slide7

Also available is the super slim plug DF59SN. This connector width is only 1.7mm as compared to the 2.7mm width of the DF59S. The DF59SN uses a common receptacle as the DF59S as well as the same floating action. Please make sure to keep sufficient insulating distance around the connector due to the exposed contact.

PTM Veröffentlicht am: