Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
usb conn
Similarly, one connector option for the USB VersaPad® is to use wire-to-board header connectors. The J7 header (Molex #53261-0471) is used for connecting external mouse buttons, the J6 (Molex #53261-0871) is the communication header. The VersaPad® is also available in a Flat Flex Cable (FFC) connector option. The FFC is used in two places: the J3 for buttons, and the J2 for the USB communication.
PTM Veröffentlicht am: