Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
theory of op
The touchpad sensor is a four-wire resistive type, composed of two resistive layers separated by an air gap. One plate is used for the X-axis and the other is used for the Y-axis. When pressure is applied, the two resistive plates make contact. A microcontroller measures this position and pressure then uses advanced, proprietary algorithms to yield smooth mouse functionality. On this slide figure 1 shows the electrical representation of the sensor. Figure 2 shows a simplified exploded view of the sensor.
PTM Veröffentlicht am: