Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Image of ITECH Electronics IT7321 Programmable AC Power Supply Introduction - Inrush Current Test

The motor contains two parts: the stator and the rotor. The stator winding is the electrical circuit of the motor, which is connected to the three-phase alternating current to produce a rotating magnetic field. The rotor obtains a certain torque and rotates under the action of the rotating magnetic field, which drives the mechanical load to work. Therefore, the motor is an inductive load and will generate a large inrush current at the moment of starting (see the figure above).

PTM Veröffentlicht am: