Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
TantCap-Slide11

Next is the definition of the category temperature and category voltage. The category temperature is the maximum recommended operating temperature of the device. To exceed the category temperature is to exceed the temperature capability of the component. The category voltage is the maximum recommended peak DC operating voltage for continuous operation at the category temperature. The example shown on this slide is a 50V rated capacitor which would now be considered 33V at 125ºC.

PTM Veröffentlicht am: