Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
FilmCap-Slide15
KEMET offers three kinds of DC link capacitors. The series C4AE is intended for low to medium power electronics applications. One or more in a bank can be used quite effectively on the same PC board which connects the IGBTs to the output converter circuits. For higher power applications there are two KEMET DC link capacitor series with screw terminal connections. These are series C44U and the low profile series C4DE. All three types offer long life in combination with high allowed ripple current.
PTM Veröffentlicht am: