Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
LEM HO 6 10 25-P Series Slide 4

The HO is an ASIC based transducer. This ASIC contains all the electronics in the transducer including the hall cell. The HO is a galvanically isolated device capable of measuring AC or DC current. It has an Over Current Detection (OCD) pin that makes it unique. The HO is available in a thru-hole with aperture package mounting style.

PTM Veröffentlicht am: