Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Varistor - Slide21 meh

In summary of this UL1449 3rd edition standard, the new safety initiative became effective in September 2009 and supersedes all preceding editions. The 3rd edition also includes new independent performance testing requirements and design considerations. The standard bases the type designations on the location of the SPD within the electrical system and component assemblies, type designators range from 1 to 5 levels. Littelfuse TMOV® Thermally protected varistors have an integrated thermally-active element to provide compliance to the abnormal overvoltage, limited current requirements of UL1449 in a single component. All ratings in the TMOV14, TMOV20, and larger devices are approved to UL1449 3rd edition. If users are uncertain on which products comply to this new standard please select the hyperlink on this slide to review and learn more.

PTM Veröffentlicht am: