Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Pt1-Slide17

There are differences between the dsPIC33 flash and dsPIC30 flash. For one thing, the dsPIC33 flash programs and erases faster than the dsPIC30 flash. The endurance of the dsPIC30 flash is greater than the endurance of the dsPIC33 flash. The dsPIC33 flash is rated for 1000 program/erase cycles. When porting programming code from a dsPIC30 system to a dsPIC33 system, the array organization is slightly different and some of the programming command codes are different.

PTM Veröffentlicht am: