Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Pt1-Slide19

The faster programming of the dsPIC33 flash allows quick programming in a factory environment. When the device is on a bulk programmer or factory board tester, the devices are fully erased in 200 milli-seconds. A large 256kB flash device can be programmed in less than 4 seconds.

PTM Veröffentlicht am: