Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
Result of Solution Conducted Emission (0.15 MHz to 108 MHz) Image of Murata's Radiated Emission Result 108 MHz Chart

Shown here are the results for radiated emission from 0.15 to 108 MHz after the use of noise counter measurements identified in the circuit diagram. The graph on the left is the result of using all the filters available, and the graphs on the right show the results of using only one of the filters. As seen, the low pass filter reduces noise at all frequencies while the common mode choke coil can significantly reduce noise above 10 MHz. By using both filters, it is possible to reduce noise greatly and to satisfy CISPR 25 Class 5.

PTM Veröffentlicht am:
PTM Updated on: 2023-01-10