Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
Common Mode Choke Technologies

Murata has three technologies used in the construction of common mode choke coils for signal lines. They consist of film, multilayer, and wirewound types. With the film type, the DLP and NFP series have the unique advantage of being small. Multilayer common mode choke coils that include the DLM and NFG series match many of the cutoff frequency requirements of high-speed interfaces, but with the added advantage of being lower cost. The wirewound type DLW series has the best performance and is also available for automotive applications. The next pages show examples of interface technologies along with Murata's common mode choke coil lineup for consumer applications.

PTM Veröffentlicht am:
PTM Updated on: 2023-01-10