Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
RS08KA2-Slide10

This is an example of an e-field sensor using the RS08KA2 to monitor the electrodes through the I/O pins. A tap or slide on an appropriate touch pad will send a signal through the e-field sensor and is read by the RS08KA2’s comparator. The ADC value is calculated using the MTIM and a table. At this point, the right response would be keyed in a touch panel screen or in a flow detection system an appropriate signal can be sent. 

PTM Veröffentlicht am: