Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
USBSypder08-Slide2

The KA, QD, and QG microcontroller families provide an entry-point into the NXP Controller Continuum which is the industry’s first and only series of compatible architectures. Each product within the continuum has family members that share packaging, peripherals, and pin-outs with the next step up or down the continuum. Common software and hardware tools create true stepwise compatibility – even across the 8-bit to 32-bit boundary.

PTM Veröffentlicht am: