Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
USBSypder08-Slide6

The Spyder08 is an in-circuit debugger, meaning it programs files into the target microcontroller and offers debugging features like real-time code execution, stepping, and breakpoints. Its debugging features use the microcontroller’s integrated Background Debug Module (BDM). The BDM communicates with the host PC board through a dedicated pin on the microcontroller. The same pin is also used during device programming.

PTM Veröffentlicht am: