Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
OSD335x C-SiP System-in-Package Family Slide 13
The C-SiP also excels in Industrial Control and Automation applications. In this example diagram, the C-SiP is managing multiple motor controls along with sensors, display and communication protocols needed for Industrial 3D printers or milling machines. With reference design support and open source libraries such as control algorithms and Open CV, no designer has to start from scratch.
PTM Veröffentlicht am: