Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
OSD335x C-SiP System-in-Package Family Slide 9
The OSD335x C-SiP now makes designing a system that runs a full operating system, such as Linux, as easy as putting down a single component, connecting power, and adding a few resistors and peripherals. As this example design diagram illustrates, that is all that is needed to have a powerful 1 GHz computer. The designer has no need to worry about complicated and tedious tasks like power sequencing or DDR routing.
PTM Veröffentlicht am: