Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Image of Octavo Systems Overview of the OSD32MP1 System-in-Package Family - Applications

There are a number of applications of the MP1 processor. For example, with the dual core A7s, it can decode video and with the 3D graphics core enabled, the customer can implement a high performance user interface. It is also possible to build AI into the product with the MP1. Using the Cortex-A subsystem, there is support for TensorFlow Lite. The AI package contains AI and computer vision frameworks and application examples. For the Cortex M real-time subsystem, there is support for STM32Cube.AI which can target the Cortex M4 in the STM32MP1. STM32Cube.AI enables mapping and running of pre-trained artificial neural networks in the real-time domain of the MP1.

PTM Veröffentlicht am: