Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Product List
Applications

The E3AS-F works well in logistics and automotive industry applications. One of the most common applications in logistics is pallet or tote positioning used for determining if a tote or pallet is in the correct position before filling the tote or pallet with goods. Additionally, in warehouses that operate using an automated storage and retrieval system (ASRS), the E3AS-F can detect the shuttle position as it moves up and down aisles and rows, stopping the shuttle at its designated storage position. Another application the E3AS-F excels in is general height detection, providing a reliable detection if an object is at the correct height. A more specific example includes detecting the sheet metal coil height to determine when the coil is nearing its end and needs to be replaced. Lastly, this sensor can be used by and large to detect difficult targets such as shiny or curved surfaces on mid or long ranges.

PTM Veröffentlicht am: