Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Product List
MEMS Flow Sensors Slide 14

Another way to develop a differential pressure in a flow channel is to use a flow cross as illustrated here. The flow sensor measures the bypass air flow, which is again proportional to the main channel flow, which is then used to calculate the total air flow in the channel using the same methods as the orifice discussed on the previous page.

PTM Veröffentlicht am: