Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Product List
MEMS Flow Sensors Slide 19

One of the advantages of the D6F-01A is that it can detect extreme low flow conditions down to 0.01% of the full-scale measurement range of the device. This equates to a flow rate of 0.1 sccm (standard cubic centimeters per minute) that can be detected with this component.

PTM Veröffentlicht am: