Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Motor Driver in White Goods Applications Slide 13

If the application calls for a stepper motor, this chart help with choosing a driver. The drivers in the shaded area are for 3 to 15 V applications and are discussed in more detail in the 3 to 15 V general purpose motor driver presentation. The higher voltage drivers at the top of the chart are discussed in the 24 V general purpose motor driver presentation.

PTM Veröffentlicht am: