Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Motor Driver in White Goods Applications Slide 5

A refrigerator designer usually has two motor selections to make. One is for the stepper motor controlling the damper, like the LV8548MC, and a two channel forward reverse brush motor driver for the automatic ice maker, like the LB1948MC. The LB1948MC & LV8548MC can actually be used in both applications because they can be configured either as a stepper motor driver or as a two channel forward reverse motor driver.

PTM Veröffentlicht am: