Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
a35us
The first of Panasonic’s solutions would include the A35US series, which is a 0.35 mm pitch connector where Panasonic has modified the fine fitting structures to be used as power terminals. Each power terminal is located on the far end of the connector and can carry up to 3 A current each. Using the movable contact construction on the header side, contact reliability of both power pins is maintained at a level that is similar to that of the smaller individual signal pins. Using this series, Panasonic can now enable 2 connections of power signals between a USB and battery in portable terminals.
PTM Veröffentlicht am: