Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
SAS-SATA-Slide17

The diagram on this slide shows the Pericom’s 4-port/8-channel SAS2/SATA3 ReDriver in a RXAUI 6.25Gb/s application in 10GE switch platforms. The ReDriver provides four high speed RXAUI interfaces, each running at 6.25Gb/s. The Pericom ReDriver is helpful in driving the external 1m RXAUI cable connected via HDMI connectors.

PTM Veröffentlicht am: