Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
PoE Slide 17

Users with SNMP may opt to access their midspan remotely by using an internet browser. Using http:// access will give users more control over administrative function such as setting the device name and password, community strings, and IP address etc. Http:// access will also allow users to update the SNMP firmware and if SNMPv3 is installed then SSL functions are also available.

PTM Veröffentlicht am: