Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
High Reliability LEDs (SMLD12 Series) (cont’d.)

Shown here are the results of high-temperature accelerated current tests conducted on the new and conventional white LEDs. In the case of the conventional product, the epoxy resin underwent a change during testing, resulting in a 20% decrease in luminous intensity, while the new product showed virtually no degradation. Under normal conditions, this translates to no significant brightness drop even after ten years, making it ideal for industrial equipment and automotive applications where long-term reliability is required.

PTM Veröffentlicht am:
PTM Updated on: 2022-09-06