Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
CSL09 Features Image of ROHM's CSL09 Series Features

These LEDs provide about 4.5 times higher luminous intensity than conventional products without a lens, allowing use as a high-brightness product, or, if the same luminous intensity is desired, they can be operated with less current. Despite utilizing a lens, the directionality is not as narrow as standard LED lamps, so even when the distance to the illuminated surface is close, there is no uneven distribution, such as spotlighting. As a result, even products that typically use LED lamps can adopt these surface-mount LEDs.

PTM Veröffentlicht am:
PTM Updated on: 2022-09-06