Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
Provisional Selection of the Motor

When making the initial provisional selection of the motor, verify that the motor holding torque is more than the load torque. If the load torque is larger than the motor holding torque, the motor will not operate normally. Verify that the load inertia is less than 10 times that of the motor. Ensuring these two points will get the designer closer to finding the correct motor for the application.

PTM Veröffentlicht am: