Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
Power Supplies 101 Slide 6

The dropout voltage of a linear regulator is the minimum voltage needed above VOUT to maintain proper regulation. An LDO is a regulator which functions when VDROPOUT is very small. The stability region of a linear regulator is the area where the output will remain stable. It is given for different output capacitances and depends on the ESR of the output capacitor.

PTM Veröffentlicht am: