Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
Power Supplies 101 Slide 7

The maximum power a device can dissipate is given by PD-MAX, which is defined as the difference between TJ-MAX and TAMBIENT divided by RTHETA-JA. It is possible to figure out what the maximum allowable output current is by combining and rearranging the power dissipation equations.

PTM Veröffentlicht am: