Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Liquid Level Reed Sensor
  • A float with a magnet rises and falls with liquid level
  • The magnet activates a reed switch when in close proximity

Coolant Truck GIF

Defining a liquid level reed sensor is quite simple. There is a float that rises and falls with the level of a liquid. The float can only float up and down in a controlled orientation. When the float reaches the detection point, whether it was rising or falling, it will activate a reed switch that is in close proximity to the float. When the float moves away from the reed switch, the contacts will open.

PTM Veröffentlicht am: