Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Liquid Level Sensing Technology Slide 5

The key component in the level sensor is the reed switch. The reed switch is hermetically sealed, which means it is impervious to any outside environment including an operating temperature range from -40°C to 200°C, and wet, moist, dirty backgrounds. The switches are then further sealed in rugged plastic with epoxy seals. Stainless steel packaging is also an option.

PTM Veröffentlicht am: