Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
Magnet Technology and Their Uses Slide 13

When magnets are to be used above 150°C, care should be taken to select magnets that are more stable at high temperatures. The most stable magnets at high temperatures are the AlNiCo series and for rare earth samarium cobalt is the best. Most magnets are relatively stable at temperatures 0°C and below, but for some magnets that is not the case.

PTM Veröffentlicht am: