Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
Magnet Technology and Their Uses Slide 26

To make a normally closed reed relay, a magnet is placed inside the coil. It is centered on the reed switch contact gap and in parallel with the switch. For maximum magnetic efficiency, the magnet is placed on the glass of the reed switch. Once in place, each of the two reeds within the reed switch become magnetized, but with opposite polarity. Being of opposite polarity, the north and the south at the reed switch gap attract each other causing the reeds to close.

PTM Veröffentlicht am: