Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
RF Reed Relays Presentation - Part 2 Slide 12

With a good RF design for a reed relay, there will be two shielded leads on each side of the signal lead. This will allow for better controlled impedance as the leads exit the relay. Shown here are the leads with the geometric dimensions still within the molded plastic. Since this is a general lead configuration, there are standard programs available to simply add the dimensions to the program, which in turn will output the exact characteristic impedance.

PTM Veröffentlicht am: