Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
RF Reed Relays Presentation - Part 2 Slide 25

The Half “T” and Full ‘T’ switching configurations will also improve isolation. In the Half T shown here there are two RF reed relays with one having open contacts and the other closed to ground. In this case, the open contacts keep the majority of the RF signal blocked and any leakage from the open contacts will be shunted to ground through the closed contacts. In the Full T there are three RF reed relays. In this case, it offers the same characteristics as in the Half T with the addition of the third relay where it further isolates the signal with its open contacts.

PTM Veröffentlicht am: