Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
DC-DC Conversion Cookbook Slide 18

Linear regulators are a special case in which the power element is driven in linear mode rather than being used like a switch ON-OFF. The power element has to absorb the difference between the input and output. The advantages are simplicity, low noise, and no inductor is used because there is no switching in the device. Although there are high current linear regulators, up to 7 A, the typical use is below 500 mA, mainly due to power losses.

PTM Veröffentlicht am: