Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
DC-DC Conversion Cookbook Slide 43

In summary, the classifications of power switching topologies are the linear step-down configuration and a switching regulator which can be built to regulate higher or lower voltage, or to invert the polarity of the supply voltage. Whether it is a linear or switching voltage regulator, the basic need is to maintain a constant output voltage at a certain load. A voltage regulator works by comparing the output voltage to an internal reference, in a closed loop feedback circuit so that the output is kept at the set value, even with variations in input voltage or load. Linear regulators are limited to a step-down configuration; switching regulators can be built to regulate higher or lower voltage, or to invert the polarity of the supply voltage, by changing the position of the FET relative to the inductor and diode in the circuit. The ST eDesign Suite is a power supply simulation tool that facilitates the selection of devices and the design of DC/DC, AC/DC, LED drivers, and photovoltaic projects. It generates interactive schematics starting from the basic design specifications.

PTM Veröffentlicht am: