Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Wireless Modules Slide 18

Other important functionality is over-the-air updates for the entire Flash file system through a specific command or update the AT Full stack firmware are the two possibilities. So from a remote server the customer can go to the module and do a firmware update. This is important because of the releasing of new versions of the firmware, so the user can always upgrade the AT Full stack. This feature is only available on the SPWF01Sx.1y models.

PTM Veröffentlicht am: