Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Wireless Modules Slide 19

ST has two different evaluation kits the USB dongle or the Wi-Fi network processor. For the USB dongle there is a Wi-Fi module and a USB connector to easily connect to a PC. Using a simple serial terminal one can test the module and send AT commands, also connect the module to the internet and do some simple test. This would be a good first step for any user to get used to the AT commands of the module. The second is a Wi-Fi module evaluation board and an STM32F0 Discovery kit. With this combination, it is possible to create an autonomous node using the Wi-Fi module. St offers firmware examples in order to do this directly on ST’s web site.

PTM Veröffentlicht am: