Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Product List
Smart Grid Solutions: Smart Grid Distribution/Smart Meters Slide 39

Shown on this slide is an implementation of the single meter. As previously described, this circuit uses the single phase energy metering device, the STPM01 with the 8-bit STM8L microcontroller for an entry level meter. An EEPROM and a 3.6 V power supply are also included in the design. This supports the IEC 61036 standard, and the LCD driver is determined by the STM8. The MCU has an RTC with calendar, data, and time built-in; there is no need for an external RTC. The EEPROM is used to data log metering parameters and any tamper event. All battery management is taken care of by the meter as well. A dual EEPROM can be used with RFID capability. An evaluation board is also available supporting low cost electricity meters and appliances.

PTM Veröffentlicht am: