Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Product List
Smart Grid Solutions: Smart Grid Distribution/Smart Meters Slide 5

The Smart Grid is a concept that applies to all the infrastructure of energy generation, distribution, and utilization. In order to make the grid smart, all three pieces of the puzzle must be in place and operational; if the Smart Meter only is considered, the grid is not very smart. It is better to understand this in terms of consumption. The right-hand side of this slide is the consumer side, where the energy is used. This portion is being made intelligent by communicating, sensing, and monitoring, either through the meter or the cloud-based infrastructure distributed inside the grid itself, to the power generation side, and back and forth. Power is generated as smart, transmitted as smart, and consumed as smart; the user becomes also an energy producer instead of simply an energy consumer and the utilities have a way to size the grid properly to what the user needs, rather than to size the grid for the peak. That is the Smart Grid.

PTM Veröffentlicht am: