Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Image of Susumu ATS Series of High-Frequency Attenuators - Slide3

The PAT series of attenuators, which are functional up to 10GHz and have been available from DigiKey, are the first attenuators Susumu introduced in the high-frequency component market. Packaging 3 resistors that form a pie circuit provided the desired attenuation, impedance matching (50 Ω), as well as significantly reduced parasitic inductance and capacitance.

PTM Veröffentlicht am: