Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
Slide12

Replacing an electrolytic capacitor with an MLCC provides various advantages such as ripple control as well as space reduction of the circuit board due to the miniature and low-profile form factor, a long lifetime and an improvement in reliability. Self-heating due to ripple currents in capacitors with a high ESR shortens the lifetime of the capacitor. The ESR of an MLCC is lower than that of an electrolytic capacitor by double-digits and the long lifetime improves the reliability.

PTM Veröffentlicht am: