Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
Slide7

Capacitor heat generation due to ESR and ripple currents is a predominant issue in the output capacitors of power supply circuits. Figure 7 shown here shows the fundamental circuit of a miniature step-down DC-DC converter which is used as a POL converter in many electronic devices. This type of output capacitor is the primary target for replacement of electrolytic capacitors with MLCCs in DC-DC converters as a solution for the self-heating issue, space reduction and improved reliability.

PTM Veröffentlicht am: