Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
dynamic-slide9

The table shown on this slide provides the TE Connectivity application tooling solutions. The contacts are standardized, reducing the number of tool types required. As can be seen, the hand crimping tool features a changeable die set structure which offers minimal installation tooling cost. Applicators for semi-automatic terminating machines are also available.

PTM Veröffentlicht am: