Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Solar Energy and SOLARLOK Slide 12

The grommet and the strain relief have been integrated into one piece. The connector comes assembled with the contact separate. It is a simple procedure to strip then crimp the wire and then snap the contact into the housing. The assembly is completed by turning the nut tight.  This is much simpler than a traditional MC connector termination.

PTM Veröffentlicht am: