Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
How to Develop an Application With Bravo? (cont’d)

Depending on which headers are soldered by the user on the Bravo board, either Arduino or Raspberry Pi boards can be mounted. The Arduino form factor supported by Bravo is “Arduino Uno”, and the application board (Arduino or Raspberry) communicates with the ME910 module through the UART port. The image depicts how the Arduino board is mounted on the Bravo.

PTM Veröffentlicht am: