Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
ESD Protection Basics Slide 10

For equipment that can be charged using a USB port, such as cell phones and tablets, it is good to have DC over-voltage protection in addition to ESD protection. This will protect the end equipment if the end user accidently grabs the wrong cable, or adapter, and applies a voltage that is too high for the USB port. The TPD1S514-1 is the most recent release, shown on this slide, which also integrates features like surge protection, over temperature protection, and integrated LDO to power the device during dead battery conditions.

PTM Veröffentlicht am: